TE 30
TE 30-AVR
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
The following symbols are used in this document:![]() |
Read the operating instructions before use. |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
Symbols in the illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
![]() |
This symbol is intended to draw special attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols are used on the product:![]() |
Drilling without hammering |
![]() |
Drilling with hammering action (hammer drilling) |
![]() |
Chiseling |
![]() |
Chisel positioning |
![]() |
Forward / reverse |
![]() |
Protection class II (double-insulated) |
![]() |
Diameter |
![]() |
Rated speed under no load |
![]() |
Revolutions per minute |
Product information
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_SYM-Logo_M_M_DEU_Hilti-Logo.jpg)
The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationCombihammer TE 30 / TE 30‑AVR Generation 02 Serial no.
Declaration of conformity
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_Konform.jpg)
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Safety
General power tool safety warnings
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_SYM-Hinweis_M_M_DEU_Gefahr.jpg)
Read all safety warnings and all instructions. Failure to follow the warnings and instructions may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference.
Work area safety
- Keep work area clean and well lit. Cluttered or dark areas invite accidents.
- Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
- Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
- Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
- Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
- Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
- Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
- When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
- If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
- Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
- Use personal protective equipment. Always wear eye protection. Protective equipment such as dust mask, non-skid safety shoes, hard hat, or hearing protection used for appropriate conditions will reduce personal injuries.
- Prevent unintentional starting. Ensure the switch is in the off‐position before connecting to power source, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
- Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
- Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
- Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
- If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
- Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
- Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
- Disconnect the plug from the power source from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
- Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
- Maintain power tools. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
- Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
- Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
- Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
Additional safety instructions for breakers
Personal safety- Use the product only when it is in technically faultless condition.
- Never tamper with or modify the tool in any way.
- When chiseling into ceilings, walls and floors, always make sure that you have a safe and firm stance. A sudden break-through can affect your balance!
- Apply appropriate safety measures at the opposite side of the workpiece in work that involves breaking through. Parts breaking away could fall out and / or fall down causing injury to other persons.
- You and any other persons in the vicinity must wear suitable eye protection, a hard hat, ear protection, protective gloves and respiratory protection while the tool is in use.
- Wear protective gloves also when changing the accessory tool. Touching the accessory tool can result in cuts and burns.
- Wear eye protection. Flying fragments can injure the body and eyes.
- Before starting work, check the hazard class of the dust that will be produced when working. Use an industrial vacuum cleaner with an officially approved protection class in compliance with the locally applicable dust protection regulations. Dust from materials such as lead-based paint, certain types of wood and concrete/masonry/stone containing quartz, minerals or metal can be harmful to health.
- Make sure that the workplace is well ventilated and, where necessary, wear a respirator appropriate for the type of dust generated. Contact with or inhalation of the dust may cause allergic reactions and/or respiratory or other diseases among operators or bystanders. Certain kinds of dust are classified as carcinogenic such as oak and beech dust, especially in conjunction with additives for wood conditioning (chromate, wood preservative). Material containing asbestos may be handled only by specialists.
- Take breaks and do physical exercises to improve the blood circulation in your fingers. Exposure to vibration during long periods of work can lead to disorders of the blood vessels and nervous system in the fingers, hands and wrists.
- Before beginning work, check the working area for concealed electric cables or gas and water pipes. External metal parts of the power tool can become live, presenting a risk of electric shock, if you accidentally damage an electric cable.
- Wait until the power tool stops completely before you lay it down.
Description
Overview of the product
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-30AVR-00001-00-01.jpg)
- Chuck
- Depth gauge release button
- Depth gauge
- Function selector switch
- Active Vibration Reduction (AVR)
- Control switch
- Grip
- Supply cord
- Forward / reverse switch
- Side handle
Intended use
The product described is an electrically powered combihammer. It is designed for drilling in concrete, masonry, wood and metal.
The version with AVR can also be used for light to medium-duty chiseling on masonry and for finishing work on concrete.- The tool may be operated only when connected to a power source providing a voltage and frequency in compliance with the information given on the type identification plate.
Possible misuse
- This product is not suitable for working on hazardous materials.
- This product is not suitable for working in a damp environment.
AVR option
The product may be optionally equipped with an Active Vibration Reduction (AVR) system, which reduces vibration noticeably.Items supplied
Rotary hammer, side handle, depth gauge, operating instructions.Technical data
Combihammer
If the device is powered by a generator or transformer, the generator or transformer’s power output must be at least twice the rated input power shown on the rating plate of the device. The operating voltage of the transformer or generator must always be within +5 % and -15 % of the rated voltage of the device.TE 30 |
TE 30‑AVR |
|
---|---|---|
Weight in accordance with EPTA procedure 01 |
4.1 kg |
4.2 kg |
Ø hammer drill bits |
6 mm …28 mm |
6 mm …28 mm |
Ø drill bits for wood |
3 mm …25 mm |
3 mm …25 mm |
3 mm …13 mm |
3 mm …13 mm |
Noise information and vibration values in accordance with EN 60745
The sound pressure and vibration values given in these instructions were measured in accordance with a standardized test and can be used to compare one power tool with another. They can also be used for a preliminary assessment of exposure. The data given represents the main applications of the power tool. However, if the power tool is used for different applications, with different accessory tools, or is poorly maintained, the data can vary. This can significantly increase exposure over the total working period. An accurate estimation of exposure should also take into account the times when the tool is switched off, or when it is running but not actually being used for a job. This can significantly reduce exposure over the total working period. Identify additional safety measures to protect the operator from the effects of noise and/or vibration, for example: Maintaining the power tool and accessory tools, keeping the hands warm, organization of work patterns.Noise emission values
TE 30 |
TE 30‑AVR |
|
---|---|---|
Sound (power) level (L WA) |
103 dB(A) |
103 dB(A) |
Uncertainty for the sound power level (KWA) |
3 dB(A) |
3 dB(A) |
Sound pressure level (L pA) |
92 dB(A) |
92 dB(A) |
Uncertainty for the sound pressure level (KpA) |
3 dB(A) |
3 dB(A) |
TE 30 |
TE 30‑AVR |
|
---|---|---|
Vibration emission value for drilling in metal |
2.6 m/s² |
4.4 m/s² |
Uncertainty |
1.5 m/s² |
1.5 m/s² |
Hammer drilling in concrete (ah, HD) |
16.8 m/s² |
9.3 m/s² |
Uncertainty (K) |
1.5 m/s² |
1.5 m/s² |
Chiseling (ah, Cheq) |
·/· |
9.2 m/s² |
Uncertainty (K) |
·/· |
1.5 m/s² |
Operation
Preparations at the workplace
Observe the safety instructions and warnings in this documentation and on the product.Fitting the side handle
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-030-AVR06-10.jpg)
- Release the side handle clamping band by turning the handle grip.
- Slide the side handle clamping band over the chuck from the front and into the recess provided.
- Bring the side handle into the desired position.
- Tighten the side handle clamping band by turning the handle grip.
Adjusting the depth gauge (optional)
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-30AVR-00005.jpg)
- Press the release button on the side handle.
- Adjust the depth gauge to the desired drilling depth.
- Release the release button.
- Check that the side handle is securely attached.
Removing the chuck
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-030-AVR04-10.jpg)
- Disconnect the supply cord plug from the power outlet.
- Grip the chuck as shown in the illustration and pull the three chuck release rings upwards.
- Lift the chuck upwards away from the tool.
Fitting the chuck
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-030-AVR04-10.jpg)
- Disconnect the supply cord plug from the power outlet.
- Grip the chuck as shown in the illustration and pull the three chuck release rings upwards.
- Fit the chuck onto the chuck mount.
- Rotate the chuck until it engages in position.
Fitting the accessory tool
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-030-AVR05-10.jpg)
- Apply a little grease to the connection end of the accessory tool.
- Use only genuine Hilti grease. Use of the wrong grease can result in damage to the tool.
- Use only genuine Hilti grease. Use of the wrong grease can result in damage to the tool.
- Push the accessory tool into the chuck as far as it will go, turning it and applying light pressure until it engages with an audible click.
- After fitting the accessory tool, grip it and pull it firmly in order to check that it is securely engaged.
- The product is ready for use.
- The product is ready for use.
Removing the accessory tool
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-030-AVR05-10.jpg)
- Pull the chuck ring back as far as it will go and remove the accessory tool.
Types of work
Check extension cords at regular intervals and replace them if found to be damaged.Function selector switch
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-30AVR-00006-10-01.jpg)
- Set the function selector switch to the desired working position.
- Do not operate the function selector switch while the motor is running. Risk of damage!
- Do not operate the function selector switch while the motor is running. Risk of damage!
Drilling without hammering
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-30AVR-00006-10-01.jpg)
- Set the function selector switch to this symbol:
.
Drilling with hammering action (hammer drilling)
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-30AVR-00006-10-01.jpg)
- Set the function selector switch to this symbol:
.
Positioning the chisel (only TE 30-AVR)
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-30AVR-00006-10-01.jpg)
- Set the function selector switch to this symbol:
.
- The chisel can be adjusted to 12 different positions (in 30° increments). This ensures that flat chisels and shaped chisels can always be set to the optimum working position.
- The chisel can be adjusted to 12 different positions (in 30° increments). This ensures that flat chisels and shaped chisels can always be set to the optimum working position.
Chiseling (only TE 30-AVR)
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-30AVR-00006-10-01.jpg)
- Set the function selector switch to this symbol:
.
Forward / reverse
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_TE-030-AVR08-10.jpg)
- Set the forward/reverse switch to the desired direction of rotation.
- Do not operate the function selector switch while the motor is running. Risk of damage!
- Do not operate the function selector switch while the motor is running. Risk of damage!
Care and maintenance
Care- Carefully remove stubborn dirt from the tool.
- Clean the air vents carefully with a dry brush.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as they can attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
- After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
Transport and storage
- Do not transport electric tools with accessory tools fitted.
- Always unplug the supply cord before storing an electric tool or appliance.
- Store tools and appliances in a dry place where they cannot be accessed by children or unauthorized persons.
- Check electric tools or appliances for damage after long periods of transport or storage.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
The tool doesn’t start or switches itself off during operation. |
Interruption in the electric supply. |
|
The carbon brushes are worn out. |
|
|
No hammering action. |
The power tool is too cold. |
|
The function selector switch is set to “Rotary drilling only” ![]() |
|
|
Contact pressure too low. |
|
|
The combihammer doesn’t achieve full power. |
The gauge (cross section) of the extension cord conductors is inadequate. |
|
The control switch is not fully pressed. |
|
|
The tool has been set to reverse rotation. |
|
|
Voltage from generator is too low. |
|
|
The drill bit doesn’t rotate. |
The function selector switch is not engaged or is in the ![]() ![]() |
|
The drill bit can’t be released. |
The chuck is not pulled back fully. |
|
Disposal
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_SYM-Hinweis_M_M_DEU_Recycling_f.jpg)
RoHS (Restriction of Hazardous Substances)
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_QRTE30.jpg)
![Image alternative](https://files-techDocs.hilti.com/2143375/H2_BILD-Objekt_System_TE_30-G2_DEU_QRTE30AVR.jpg)
There is a link to the RoHS table, in the form of a QR code, at the end of this document.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.